Children's of Alabama, Birmingham, Alabama, Estados Unidos

abril 14, 2021 porSensormaticTeam

Compartir

Challenge

Ranked as one of the best pediatric medical centers in the nation, Children’s of Alabama holds a valuable position as the only medical center in Alabama dedicated solely to the care and treatment of children and is a Level 1 state designated trauma facility.

In 2008, the non-profit hospital sought a way to maximize energy savings in their new 14-story patient tower in the heart of Birmingham.

Emphasizing the need to be good stewards of financial donations, the hospital sought a partnership to find innovative solutions to drive maximum efficiency of operations, lower energy costs, reduce risk of failure, and provide guaranteed outcomes.

Solutions

OpenBlue Central Utility Plant Program: The hospital looked to Johnson Controls to design, build, operate and maintain its new central utility plant (CUP) through a 25-year contract where Johnson Controls operates and holds all the risk for building systems.

Children’s of Alabama is an early adopter of OpenBlue Enterprise Manager.

Results

  • By meeting or exceeding yearly performance guarantees, Johnson Controls has provided nearly $250,000 in annual savings.
  • Reduced the use of natural gas by 69%.
  • When complete, Children’s of Alabama expects this portion of the project to save $450,000 a year.

Learn more about the work we do

Download the full case study

Related Items

People walking along a bridge in a business park, with OpenBlue graphics overlaid in the background

Healthy Buildings

Johnson Controls Healthy Buildings generate returns while creating healthy, sustainable environments that drive occupant well-being.

Cityscape overlaid with graphics depicting transmission nodes

OpenBlue

Applying data from both inside buildings and beyond, our customers can now manage operations systemically.

Johnson Controls technician using a tablet and inspecting HVAC equipment

Central Utility Plant Optimization

We build on our innovative OpenBlue digital platform to connect systems and data for intelligent, automated decision-making. See rapid ROI, drive down costs, increase reliability and advance your sustainability goals.