New IQ Remote PowerG security panel from Johnson Controls offers superior range and reliability of control

IQ Remote PowerG security panel product image

The IQ Remote PowerG is a secondary control panel that gives customers the power to control their security and smart home system with the superior range and reliability of PowerG technology.

Share

ISC West attendees can stop by the Johnson Controls stand 18033 during the show March 29-31 to learn more about the IQ Remote PowerG control panel

MILWAUKEE – (March 27, 2023) –  Johnson Controls, the global leader for smart, healthy and sustainable buildings, today announces the new IQ Remote PowerG Security Panel. The IQ Remote PowerG is a secondary control panel that gives customers the power to control their security and smart home system with the superior range and reliability of PowerG technology.

Johnson Controls will showcase the IQ Remote PowerG Security Panel as part of an entire suite of security solutions in stand 18033 at ISC West, March 29 to 31 at the Venetian Expo in Las Vegas, Nevada.

IQ Remote PowerG empowers users to fully utilize security and smart ecosystems wherever they need with PowerG’s reliable connectivity.

— Jonny Safford, commercial marketing manager for Johnson Controls

“IQ Remote PowerG empowers users to fully utilize security and smart ecosystems wherever they need with PowerG’s reliable connectivity,” said Jonny Safford, commercial marketing manager for Johnson Controls. “Incorporating PowerG is an important step in providing customers with convenient, speedy access to their systems in large residential and commercial installations.”

Customers can add up to eight IQ Remote PowerG panels per system. The 7-inch LCD touchscreen mirrors the elegant user interface of the main IQ Panel 4, providing access to their system and ease of use wherever it is set up. IQ Remote PowerG features the same chimes, voices and alarm sounds as IQ Panel 4, as well as the ability to view video streams from cameras doorbells with the Live View, Live Answer feature.

IQ Remote PowerG is also compatible with the powerful new IQ Pro, a hybrid wired/wireless system built for larger residential, business and commercial installations.

Additional features include PowerG Security Radio for reliable, encrypted, long-range wireless communications, OTA upgrades allowing for future enhancements, emergency panics, and live view video cameras and video doorbell (Wi-Fi required). The IQ Remote PowerG Control Panel is UL 2610 and ULC-S304 rated, including 24-hour backup battery. Users can pair up to three panels over Wi-Fi and five panels over PowerG for a total of eight panels.

Attendees can stop by the Johnson Controls stand (18033) at ISC West to learn about the IQ Remote PowerG and other residential and commercial security solutions. For more information, visit Johnson Controls at ISC West or go to www.johnsoncontrols.com/security.

To preorder the IQ Remote PowerG, find and contact your local distributor here: https://qolsys.com/find-a-distributor/.

Media Contact:
Karen Tognarelli
Director, Public Relations & Media
Direct: +1 571.214.7744

###

About Johnson Controls:

At Johnson Controls (NYSE:JCI), we transform the environments where people live, work, learn and play. As the global leader in smart, healthy and sustainable buildings, our mission is to reimagine the performance of buildings to serve people, places and the planet.

Building on a proud history of nearly 140 years of innovation, we deliver the blueprint of the future for industries such as healthcare, schools, data centers, airports, stadiums, manufacturing and beyond through OpenBlue, our comprehensive digital offering.

Today, with a global team of 100,000 experts in more than 150 countries, Johnson Controls offers the world’s largest portfolio of building technology and software as well as service solutions from some of the most trusted names in the industry.

Visit www.johnsoncontrols.com for more information and follow @JohnsonControls on social platforms.

Share